Part Number: LSF0204
Tool/software:
Does LSF0204 support hot-swap?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
That depends on your definition of "hot-swap". Is it the LSF0204 itself or only the other devices that are powered down and hot-swapped? What do you want to happen when some device is (un)plugged? When exactly should that happen?
The LSF isolates the two sides only if the EN pin is forced low.
Hello Cain,
Our apps team is current out today celebrating Labor Day (US Holiday). Allows us two days to respond back. Thank you for your understanding.
Regards,
Josh
Hi Clemens,
Thanks for your replys, We are using LSF0204 to Isolate GPIO signal, and place it between the connector and SOC. A key requirment here is that the connector needs to support hot-swap---meaning it may be unplugged or plugged in while the device is power on.
Hi Cain,
Similar to Clemens' response, the LSF can be used for hot-swap application if the bus is being connected properly (order should be ground, VCC, and then data).
Please keep in mind that hot-swap application typically involves longer traces and connector lengths- since the LSF0204 is a passive translator with no buffering it will not be able to redrive the signals through higher capacitances.
Regards,
Jack