This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

THVD2410: PSPICE Model

Part Number: THVD2410

Tool/software:

Hey team,

Do we have a PSPICE model for this part? I'm not seeing one on PSPICE or our website.

Thanks,

Cam

  • Hi Cam,

    So we don't officially release most of our spice models for RS-485 because we don't have many and we don't have a focus on making spice models as most people do not need them since these are relatively simple devices. 

    However - you are in luck on this specific device as we do have a library file (this is the base of the Pspice model - they will need to create an .OLB file when importing the .lib file into Pspice (it is just the symbol associated with the .lib file - pspice models are a .lib file + symbol file (.olb) - the logic of the model is all in .lib file). 

    This library is compatible with Tina and Pspice - but not LTSpice (syntax is slightly different). 

    thvd2410.lib

    It is a typical only model - so stress testing isn't really possible on this device. The device is also very linearized from the model P.O.V. 

    Please let me know if you have any other questions. 

    Best,

    Parker Dodson