Part Number: SN65DP149
Other Parts Discussed in Thread: SN65DP159, TDP158, TMDS181, TMDS171, TDP0604, TDP1204
Tool/software:
Hi,
I noticed that most retimer/redriver are in a QFN 40 or QFN 48 capsule.
I think i found a few combination where they are drop in replacements.
So is there a list of drop in replacement parts?
like IC1 2 3 4 are drop in replacements for each other
Also is there a guide to when to use a HDMI retimer vs redriver and IF i need any to begin with?
I am asking since i was thinking that if i get a pair of drop in replacement chips where one is a retimer and
the other is a redriver i can test both with the same PCB and in production use the most suitable one.
As a note as of now i am just in the planning stage and i dont know the input and output cable length and type.
As for HDMI speed i need HDMI 1.3 or better (1.2 would be enough but i want some space for later upgrades in terms of monitor ).
Also is there any way to estimate HMDI cable loses ? Asking since i might be able to bet cable length estimates in the near future.
Best regards,
Robert