Part Number: TUSB9261
Tool/software:
Hi,
I wonder if the TUSB9261 can be powered only by a USB 3.0 (+5V), or do I need to connect the +1,1V and +3,3V pins?
The way I understood it is that the TUSB9261 can be powered via USB_VBUS (pin 50) and can leave the +1,1V and +3,3V pins unconnected.
Best regards,
Andreas