This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSB4041I: 3.3V is back feeding onto 1.1V rails

Part Number: TUSB4041I
Other Parts Discussed in Thread: TPS65220,

Tool/software:

Hi, we're using the TUSB4041IPAPR and TPS65220 is the PMIC for our processor.  This PMIC design has 3.3V rail coming up before the 1.1V rail, which looks fine from the datasheet as long we come out of reset after the rails have settle.  The hub works as designed.  The issue we're having is that the 3.3V on the Hub is back feeding onto the 1.1V before the 1.1V rail has been turned on by the PMIC.  We're seeing around 0.25V on this rail and in some edge cases this voltage is high enough that the PMIC will not turn on.