Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83867IR: 1Gbps link fails with specific cables

Part Number: DP83867IR

Tool/software:

Hi everyone,

I'm having some problems with the DP83867IR PHY and certain Ethernet cables. Our product is in mass production stage and some units over thousands experience this behaviour.

Let me explain with a practical example.

I have three different Ethernet cables, which I will call A, B and C.

The PHY links at 1 Gbps with cables A and B, but only at 100 Mbps with cable C.

The same cables are used to connect other products of the same model (same PHY, same electronics, same layout), and all of them link at 1 Gbps with cables A, B and C.

This test is highly reproducible, even with different NICs.

I have read almost all of the PHY registers, but nothing seems suspicious.

Here are some registers when the camera is connected via cable C (the one that connects at 100 Mbps)

name address value
BMCR 0x0000 0x1140
BMSR 0x0001 0x7949
PHYIDR2 0x0003 0xA231
ANAR 0x0004 0x0D81
ANLPAR 0x0005 0xCDE1
ANER 0x0006 0x0064
ANNPTR 0x0007 0x2001
ANNPTR 0x0008 0x0000
CFG1 0x0009 0x0300
STS1 0x000A 0x0000
PHYSTS 0x0011 0x0302
ISR 0x0013 0x0040
RECR 0x0015 0x0000
BISCR 0x0016 0x0000
STS2 0x0017 0x0040
CFG3 0x001E 0x0002
CRE 0x008A 0x0000
ALTFGAB 0x00A0 0x0908
ALTFGCD 0x00A1 0x060A
RXFSTS 0x0135 0x0000
IO_MUX_CFG 0x0170 0x0C0E

TDR done with cable C connected and NIC disabled:

name address value
TDR_PEAKS_SIGN_A_B  0x01A5 0x0021 (with cables A, B the value is 0x0021)
TDR_PEAKS_SIGN_C_D 0x01A6 0x0061 (with cables A, B the value is 0x0021)

Do you have any suggestions?

Thank you in advance for your time.

Regards.

  • Hi Mirko, 

    It looks like the link is disabled in the register dump. But, you are seeing that the link is up and is 100Mbps, right?
    Also, what are the cable length?

    Best,
    J

  • Hi J,

    I apologise; I attached the register dump that was performed during the TDR, so the connection was down. For completeness, here is the one with the link up at 100Mbps with the cable C.

    name address value
    BMCR 0x0000 0x1140
    BMSR 0x0001 0x796D
    PHYIDR2 0x0003 0xA231
    ANAR 0x0004 0x0D81
    ANLPAR 0x0005 0xCDE1
    ANER 0x0006 0x006F
    ANNPTR 0x0007 0x2001
    ANNPTR 0x0008 0x6001
    CFG1 0x0009 0x0300
    STS1 0x000A 0x2800
    PHYSTS 0x0011 0x6F02
    ISR 0x0013 0x1800
    RECR 0x0015 0x0000
    BISCR 0x0016 0x0000
    STS2 0x0017 0x0040
    CFG3 0x001E 0x0002
    CRE 0x008A 0x0000
    ALTFGAB 0x00A0 0x0908
    ALTFGCD 0x00A1 0x060A
    RXFSTS 0x0135 0x0000
    IO_MUX_CFG 0x0170 0x0C0E

    The cables are in range of 1-10 m, the cable C is 10 m.

    I'd also like to mention that I tried the improvements suggested in Section 3 of the SNLA246C: '3.2 Improving Link Margins across Different Channels' and '3.4 Unstable Link Up Debug in 1 Gbps Communication'. However, these make small improvements, sometimes the PHY links at 1Gbps sometimes at 100Mbps with cable C.

    ---

    Moreover, I read MSE registers as suggested in SNLA246C.

    This is a case in which the PHY links at 1Gbps with cable C. 

    MSE_A 0x0225: 0x0091

    MSE_B 0x0265: 0x01C5

    MSE_C 0x02A5: 0x003B

    MSE_D 0x02E5: 0x0041

    ---

    Sometimes happens the following situation:

    when connecting the ethernet cable the MSE registers has these values for just one read (every 1 second):

    MSE_A 0x0225: 0x014F

    MSE_B 0x0265: 0x034E

    MSE_C 0x02A5: 0x0064

    MSE_D 0x02E5: 0x006B

    And then, these registers has the followings values:

    MSE_A 0x0225: 0x0076

    MSE_B 0x0265: 0x7FFF

    MSE_C 0x02A5: 0x7FFF

    MSE_D 0x02E5: 0x7FFF

    Thus, the PHY links at 100Mbps.

    Hope this could help.

    ---

    Regards,

    Mirko

  • Hi Mirko, 

    Interesting, it seems like this cable has a particularly bad link quality on line B before the link drops to 100M. 
    Could you also try the script on 3.1 of SNLA246C?

    I looked at your TDR results, but we would need more information to analyze the TDR results. 
    If you can, could you run another TDR because we need the results from the following registers besides 1A5 and 1A6:


    This is from this application note if you are interested to do the analysis yourself, but please share the results so I can also do the analysis myself and we can see what could be wrong with this particular cable, or if there are any issues on the PHY. 

    Also, what is the length of cable C? And, does this cable work fine if it is used for other links?

    Best,
    J

  • Hi J,

    I tried the script on 3.1 of SNLA246C but it does not make any difference.

    Here it is the complete TDR registers:
    0x0190: 0x000F
    0x0191: 0x0000
    0x0192: 0x1000
    0x019A: 0x002B
    0x019B: 0x0000
    0x019C: 0x2400
    0x01A5: 0x0021
    0x01A6: 0x0061

    ---

    Cable C is 10 metres long. It works fine for other links, even at 10 Gbps.

    I also tried a 100 m cable, but it wouldn't connect at all, even at 100 Mbps.

    Regards,

    Mirko

  • Hi Mirko, 

    TDR result didn't yield much information unfortunately. 

    In the meantime, have you tried writing 0xF508 to register 1D5h? This is supposed to increase the voltage swing of the PHY in 1G. I wonder if this issue relates to the voltage swing. 
    What is the cable length and type of cable A and B? For cable C, what is the cable type of cable C?

    Would it also be possible to look at the schematic/layout to check all the grounds? Feel free to share them via private message. I've sent you friendship request.

    How many units have been affected by the way?

    What are the link partners you have tested?


    Best,
    J

  • Hi J,

    I accidentaly hit the "This resolved my issue" button.

    By the way, I already tried writing 0xF508 to register 1D5h, and this is one of the changes that let the PHY link at 1Gbps even with cable C sometimes. But it does not resolve the issue completely.

    Cable A is 0.5 m CAT5E, cable B is 5 m CAT6, cable C is 10 m CAT6.

    Until now more or less 5 units have been affected over thousands.

    The link partners I tested are various, Intel, Realtek, 1G and 10G. Do you need more details on this?

    I'll collect the schematics/layout and send them to you via private message, thank you!

    Regards,

    Mirko

  • Hi Mirko, 

    I see. You can get additional increase of VoD swing using registers 0xA0 and 0xA1. However, the increase depends on the trim of the PHY. 
    Since it is 5 out of 1000s of boards, could we try doing a ABA swap on the problematic PHY? This will isolate if this is the PHY or the board issue. 
    Once you send me the design files, I can look at them to see if there's anything that is out of our recommendation also. 

    Please let me know. 

    Best,
    J


  • Hi J,

    I have already tried increasing the VoD via registers 0xA0 and 0xA1, but it made no difference.

    I'm sending you the schematics and layout of the PHY parts.

    In the meantime, we tried an ABA swap, and found that the issue followed the PHY. The board with the new PHY can now link at 1 Gbps with all cables, whereas a different board with the suspected PHY can only link at 100 Mbps.

    Regards,

    Mirko

  • Hi Mirko, 

    Since the issue follows the PHY during ABA swap, we are suspecting this could be a quality issue. I will check your design and get back to you if there are any design flaws that could be causing this, but in the meantime, could you submit a return request through the FAE for failure analysis?

    Best,
    J

  • Hi Mirko, 

    I noticed a few things on the schematic: 

    1. MDC line doesn't require 2.2k pullup. 
    2, I noticed that mirror mode is meant to be enabled but it seems like LED0 is not strapped to mode 3. Could you confirm?

    Best,
    J

  • Hi J,

    1. We interpreted the MDIO as an I2C-like communication protocol, so the MDC line is pulled up. Could this lead to errors?

    2. LED_0 (pin 47) is unconnected to disable Mirror Mode. There is a note in the schematic explaining the function of each pin, as well as the actual configuration.

    Regards,

    Mirko

  • Hi Mirko, 

    MDIO is similar to I2C, but the specification does not require a pull-up on MDC. I've seen previous customer designs with pull-ups on MDC and it works fine. In your case also, most PHYs are working properly so I do not expect this will lead to errors, but I've given the feedback more as FYI. 

    I apologize for the confusion on mirror mode. I misread the strap configuration as you meant to enable mirror mode. That makes sense as it matches the pinout on the PHY. The transformer was inverted that I misunderstood. 

    Were you able to submit a return request?

    Best,
    J

  • Hi J,

    We got the PHY from Arrow. But they're not supporting TI anymore.

    Do you know how I should go about making a return request?

    Thanks!

    Regards,

    Mirko

  • Hi Mirko,

    Please use this link to reach out to Customer Support. 
    You will have to make TI account and feel free to refer to this E2E thread that the team asked you to submit for return. 

    Best,
    J

  • Hi J,

    we will proceed with a return request.

    Thank you for your time!

    Regards,

    Mirko

  • Hi Mirko, 

    Thank you for your update. Please feel free to reply to this thread, or open a new thread if any application problem arises. 

    Best,
    J