Other Parts Discussed in Thread: TCA9511A, TCA9617B, TCA9509, TCA9548A
Tool/software:
Hi,
two questions about TCA9617.
1. Can TCA9617 B side work with TCA9511 A side? Consider of Vol voltage.
2. I see Vol of TCA9617 B side is 0.58v max when IoL=30mA. that means the B side driver has a 20ohm resistance, and the actual Vol will be divided with the external pull up resistor. Or the B side has a fixed Vol= 0.53?