This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN65MLVD2: Absolute Maximum Operating Junction Temp

Part Number: SN65MLVD2

Tool/software:

Hi, I refer to SN65MLVD2DRBT (https://www.ti.com/product/SN65MLVD2/part-details/SN65MLVD2DRBT?keyMatch=SN65MLVD2DRBT&tisearch=universal_search&usecase=OPN

I understand from the datasheet that the device is characterised for operation up to +85degC. I suppose this is the ambient air temperature. 

I would like to check if a maximum operating junction temperature is available? 

Thank you 

  • Hi Benedict,

    So it isn't directly spec'd but you can derive it to be 125C. 

    From this table we can derive R_theta_JA - which is the thermal ambient to junction impedance. 

    There are two values here - one for a Low-K and one for a high-K PCB. 

    If you take the inverse of the derating factor above TA = 25C  - that is the R_theta_JA value. 

    So for Low-K R_theta_JA = 357.14 C/W

    For High-K R_theta_JA = 151.06 C/W

    We also know that:

    TJ = TA + P*R_theta_JA 

    and we are also given power ratings

    If we plug in the max ambient temperature allowed + the max power dissipation of IC from chart we can get the max TJ - or the max junction temperature. 

    So 

    High K PCB --> TJ = 85 + 112mW * 357.14 = 125C

    Low K PCB --> TJ = 85 + 264mW * 151.06 = 125C

    So since our max power ratings and the thermal to ambient junction impedance are spec'd we can derive max allowable junction temperature to 125C for this device. 

    Best,

    Parker Dodson

  • Hi Parker, genius! Thanks for this, I will pay more attention to the datasheet in future.