Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMDS1204EVM: Optimal AC-Coupled Mode Setup & I2C Register Programming for Basic Sanity Testing

Part Number: TMDS1204EVM
Other Parts Discussed in Thread: TMDS1204, TDP1204,

Tool/software:

Hi everyone,

I'm working with the TMDS1204 HDMI redriver EVM and need guidance on setting it up in AC-coupled mode with I2C programming for basic sanity and stability testing. I want to pass a signal from a PC video source through to an HDMI sink/display for validation and oscilloscope probing.

Hardware Setup:

  • PC HDMI output → TMDS1204 EVM input

  • TMDS1204 EVM output → HDMI display (or breakout adapter for scope measurements)

  • Using Aardvark I2CSPI host for register programming

Current Configuration Questions:

  1. AC-Coupled Mode Setup: For sink-side applications, I believe I need:

    J27 jumper: Short 1 to 2 (AC_EN enabled)

    Ensure 100nF capacitors are populated on OUT_D[2:0] and OUT_CLK lanes

    499Ω pull-down resistors to ground after coupling caps

  2. Essential I2C Register Programming:
    What's the minimal register configuration needed for reliable signal pass-through? Based on the datasheet, I'm thinking: 

    0x09, 0x00 // Exit power-down (PDEN = 0)
    0x0A, 0x00 // Enable rate and TXFFE snooping
    0x0D, 0xA3 // Linear mode, DC-coupled TX, 0dB DCG, 100Ω term
    0x0E, 0x97 // CTLE selection for HDMI 1.4/2.0/2.1
    0x11, 0x0F // Enable all four lanes

  3. DDC/HPD Configuration:
    Should I enable the DDC level shifter (J31: short 2-3) and ensure proper HPD routing (populate R131, depopulate R129) for standard operation?

Specific Goals:

  • Achieve basic video pass-through from PC to display

  • Enable oscilloscope probing of TMDS lanes at output

  • Maintain link stability for various HDMI modes (1.4/2.0/2.1) but primarily for HDMI 2.1

  • Minimize register complexity while ensuring reliable operation

Questions:

  • Are there any critical registers I'm missing for AC-coupled operation?

  • What's the recommended approach for EQ settings in a sink application?

  • Should I disable certain features (like AEQ) for initial testing?

  • Any specific considerations for different HDMI data rates?

Any insights from those who've successfully configured the TMDS1204 in similar setups would be greatly appreciated!

Thanks in advance!