This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB948-Q1: LINK issues

Part Number: DS90UB948-Q1

Tool/software:

Hello team,

My customer met some link issues when debugging 947+948, it is dual port STP connection from host to display, it is configured as automatically identification in 947 and 948 registers, the link ready status is found as single link ok. If configure the host side as dual link, it is reported as no ready.

Pls help analyze it, thanks!

BR,

Daniel 

  • Hi Daniel,

    How are they testing link and LOCK status? Please check the SER register 0xC and DES LOCK pin output.

    Also, what pixel clock rate is used? Note that clock rates supported will vary in single or dual-link modes: "The device supports OpenLDI clocks in the range of 25 MHz to 96 MHz over one lane, or 50 MHz to 170 MHz over two lanes."

    Best regards,
    Ikram

  • Hello Ikram,

    We test register 0x5A of 947, and the read data is 0x1d. According to the DS description, it is Single Link, DES LOCK is high, and the clock rate is approximately 68MHz. Display resolution: 1920*1080@60Hz. The register configuration is:

    board.WriteI2C(UB947,0x5B,0x03)

    board.WriteI2C(UB947,0x40,0x10)

    board.WriteI2C(UB947,0x41,0x49)

    board.WriteI2C(UB947,0x42,0x16)

    board.WriteI2C(UB947,0x41,0x47)

    board.WriteI2C(UB947,0x42,0x20)

    board.WriteI2C(UB947,0x42,0xA0)

    board.WriteI2C(UB947,0x42,0x20)

    board.WriteI2C(UB947,0x42,0x00)

    board.WriteI2C(UB947,0x41,0x49)

    board.WriteI2C(UB947,0x42,0x00)

    board.WriteI2C(UB947,0x03,0xDA)

    board.WriteI2C(UB947,0x17,0x9E)

    board.WriteI2C(UB947,0xC6,0x21)

    Mode_SEL configuration :

    OLDI_DUAL: Dual-pixel OpenLDI interface.

    REPEATER:  repeater mode

    MAPSEL:SPWG bit mapping

    COAX: Enable FPD-Link III for twisted pair cabling

     BR,

    Daniel

  • Hi Daniel,

    Do you have the system setup for dual link, with both DOUT0 and DOUT1 connected to the 948? Please test with pattern generation with internal clock see if there is LOCK in dual-link mode.

    Also, please check the mode straps for both SER and DES.

    Best regards,
    Ikram

  • Hello Haque,

    Do you have the system setup for dual link, with both DOUT0 and DOUT1 connected to the 948? Please test with pattern generation with internal clock see if there is LOCK in dual-link mode.

    Pls. see the attachment.

    import time
    
    # System dependant variables - adjust according to system
    UB947 = 0x18        # 947 I2C Address
    UB948 = 0x68        # Remote 948 Address
    
    
    def pollstate():
        count = 0
        board.WriteI2C(UB947, 0x23, 0x80)
        board.WriteI2C(UB947, 0x24, 0x80)
        mask = int('11111', 2)
        state = board.ReadI2C(UB947, 0x24, 1)
        while (state & mask) != 27:  # 27 = 5'b11011
            time.sleep(0.01)  # 10ms delay
            state = board.ReadI2C(UB947, 0x24, 1)
            count = count + 1
            if count == 10:
                print
                "Error: Serializer is not in Normal state"
                return (1)
    
        board.WriteI2C(UB947, 0x23, 0x0)
        board.WriteI2C(UB947, 0x24, 0x0)
    
    board.WriteI2C(UB948,0x4A,0x01) # Disable OLDI outputs on 948 to prevent screen glitches from appearing during the init process
    
    ##### Init A Sequence
    
    board.WriteI2C(UB947,0x5B,0x03) # Force dual FPD-Link, disable reset on PLL frequency change
    
    board.WriteI2C(UB947,0x16,0x02) # Adjust BCC watchdog timer to minimum
    
    board.WriteI2C(UB947,0x04,0x90) # Prevent AVMUTE for non-HDCP systems
    
    state_error = pollstate()  # Poll 947 state machine
    
    if state_error == 1:
        print "Serializer not in normal state"
    
    board.WriteI2C(UB947,0x40,0x10)
    board.WriteI2C(UB947,0x41,0x49)
    board.WriteI2C(UB947,0x42,0x16)
    board.WriteI2C(UB947,0x41,0x47)
    board.WriteI2C(UB947,0x42,0x20)
    board.WriteI2C(UB947,0x42,0xA0)
    board.WriteI2C(UB947,0x42,0x20)
    board.WriteI2C(UB947,0x42,0x00)
    board.WriteI2C(UB947,0x41,0x49)
    board.WriteI2C(UB947,0x42,0x00)
    
    time.sleep(0.01)
    
    board.WriteI2C(UB948,0x01,0x01) # Digital reset to restart AEQ
    time.sleep(0.1) # Allow time for 948 to relock
    board.WriteI2C(UB948,0x4A,0x00) # Enable OLDI outputs on 948
    
    #User defined programming sequence
    
    board.WriteI2C(UB947, 0x03, 0xDA)
    board.WriteI2C(UB947, 0x17, 0x9E)
    board.WriteI2C(UB947, 0x4F, 0x80)
    board.WriteI2C(UB948, 0x26, 0x16)
    board.WriteI2C(UB948, 0x27, 0x16)
    
    #PATGEN programming
    
    board.WriteI2C(UB947,0x64, 0x10) //disabled patttern
    board.WriteI2C(UB947,0x66, 0x04)
    board.WriteI2C(UB947,0x67, 0xbc)
    board.WriteI2C(UB947,0x66, 0x05)
    board.WriteI2C(UB947,0x67, 0xa7)
    board.WriteI2C(UB947,0x66, 0x06)
    board.WriteI2C(UB947,0x67, 0x45)
    board.WriteI2C(UB947,0x66, 0x07)
    board.WriteI2C(UB947,0x67, 0x80)
    board.WriteI2C(UB947,0x66, 0x08)
    board.WriteI2C(UB947,0x67, 0x87)
    board.WriteI2C(UB947,0x66, 0x09)
    board.WriteI2C(UB947,0x67, 0x43)
    board.WriteI2C(UB947,0x66, 0x0a)
    board.WriteI2C(UB947,0x67, 0x14)
    board.WriteI2C(UB947,0x66, 0x0b)
    board.WriteI2C(UB947,0x67, 0x02)
    board.WriteI2C(UB947,0x66, 0x0c)
    board.WriteI2C(UB947,0x67, 0x14)
    board.WriteI2C(UB947,0x66, 0x0d)
    board.WriteI2C(UB947,0x67, 0x08)
    board.WriteI2C(UB947,0x66, 0x1a)
    board.WriteI2C(UB947,0x67, 0x09) //M=9
    board.WriteI2C(UB947,0x66, 0x03)
    board.WriteI2C(UB947,0x67, 0x35) //N=53
    board.WriteI2C(UB947,0x65, 0x04) //internal clk and timing
    board.WriteI2C(UB947,0x64, 0x41)

    Also, please check the mode straps for both SER and DES.

    Refer to the setting of 947 internal pattern in 947_Init.py, it cannot enter dual-link mode.

    Thanks

    BR,

    Daniel

  • Hi Daniel, please give me 1-2 days to check this and get back to you.

    Best regards,
    Ikram

  • Hi Daniel,

    Could you send a photo of the setup and check if both DOUT0 and DOUT1 are connected between SER and DES.

    Also, after you run the script, is there LOCK and clock output detected from the 948? The 948 should have LOCK with PATGEN enabled, in both single and dual link modes. You can check the LOCK output on DES 948 pin.

    Best regards,
    Ikram