Tool/software:
Hi,
I would like to confirm the recommended handling of the USB_VBUS pin (Pin16) on TUSB4041.
In our system, we do not use the USB-PD negotiated 20 V rail directly, and we do not require upstream 5 V VBUS detection.
In this case, is it acceptable to leave Pin16 (USB_VBUS) unconnected (NC)?
Or, should we always provide the 5 V rail through the recommended resistor divider (90.9 kΩ / 10 kΩ) as described in the datasheet?
Could you please advise the recommended connection method for this pin when VBUS detection is not required?
Best regards,
Conor