Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TCAN4550-Q1: Need TCAN4550-Q1 vxworks driver source code

Part Number: TCAN4550-Q1
Other Parts Discussed in Thread: TCAN4550

Tool/software:

Hello,

I’m working with the TCAN4550-Q1, which is connected to a T2081 processor via SPI. I’ve already tested it under Linux, but now I need to implement it on VxWorks. Since VxWorks doesn’t provide a built-in driver for the TCAN4550, I need a driver for it. Could you provide me with the TCAN driver for VxWorks?

Regards

Ravindra Arumilli