Part Number: DS320PR810
Tool/software:
I am trying to configure the DS320PR810 redriver through SMBus using an MCU programmed to write to the memory addresses of the redriver's registers.
I have 2 redrivers, one for each direction that are configured to have addresses using the EQ/ADDR pins with (L0, L0) for one and (L1, L1) for the other.
So there are actually 2 sets of addresses in each of them. The memory address mode that they operate with is 8bit from what I read.
I just defined some constants in the C code for the addresses and various configuration values and then I use them in the MCU C functions for communicating with the redriver.
In my case, there is more loss in a direction, from GPU to CPU and for the other way around, CPU to GPU there is less loss and I just want it to act as a basic signal conditioning without anything fancy.
Bellow is the code for configuring the redrivers, and I am curious if I need to configure anything else besides what is written bellow and if the code seems alright. Also, I could not find enough information about the EQ profiles and which ones should I use. I guess this is based on the medium used for transmission of the pcie signal, in my case being cable + PCB
I am assuming that each channel has a unique address and from that address I have the same offsets that I need to write to across all channels. For example, if I want to write to channel 0 the eq settings, I would need to write to the channel_0_Address + eq_offset_address.
Also, I saw that some registers have reserved bits so I am not doing anything with them but I am writing 0 to them, maybe I should first read the values from registers with reserved bits and only change the ones that I need, writing back to the register the previous read value with only the changed bits that I am interested in.
#include "main.h"#include <stdio.h>#include <string.h>#include <stm32f0xx_hal_i2c.h>extern I2C_HandleTypeDef hi2c2;#define CPU_GPU_0_3_ADDR_I2C 0x18#define CPU_GPU_4_7_ADDR_I2C 0x19#define GPU_CPU_0_3_ADDR_I2C 0x22#define GPU_CPU_4_7_ADDR_I2C 0x23#define CHANNEL_0_REGISTER 0x00#define CHANNEL_1_REGISTER 0x20#define CHANNEL_2_REGISTER 0x40#define CHANNEL_3_REGISTER 0x60#define CHANNEL_4_REGISTER 0x00#define CHANNEL_5_REGISTER 0x20#define CHANNEL_6_REGISTER 0x40#define CHANNEL_7_REGISTER 0x60#define EQ_CONTROL_REGISTER_OFFSET 0x01#define EQ_CONTROL_EQ_STAGE1_BYPASS 0x80#define EQ_CONTROL_EQ_STAGE1_3 0x40#define EQ_CONTROL_EQ_STAGE1_2 0x20#define EQ_CONTROL_EQ_STAGE1_1 0x10#define EQ_CONTROL_EQ_STAGE1_0 0x08#define EQ_CONTROL_EQ_STAGE2_2 0x04#define EQ_CONTROL_EQ_STAGE2_1 0x02#define EQ_CONTROL_EQ_STAGE2_0 0x01#define EQ_GAIN_FLAT_GAIN_REGISTER_OFFSET 0x03#define EQ_PROFILE_3 0x40#define EQ_PROFILE_2 0x20#define EQ_PROFILE_1 0x10#define EQ_PROFILE_0 0x08#define FLAT_GAIN_2 0x04#define FLAT_GAIN_1 0x02#define FLAT_GAIN_0 0x01#define RX_DETECT_CONTROL_REGISTER_OFFSET 0x04#define MR_RX_DET_MAN 0x04 //force always detect#define EN_RX_DET_COUNT 0x02 //enable additional rx detect polling#define SEL_RX_DET_COUNT 0x01 //enable additional rx detect 0 = 2 valid detections, 1 = 3 additional valid detections#define BIAS_REGISTER_OFFSET 0x06#define BIAS_CURRENT_2 0x20#define BIAS_CURRENT_1 0x10#define BIAS_CURRENT_0 0x08static void initialize_channel_eq(uint16_t redriver_address, uint16_t channel_register_address, uint8_t eq_index) { HAL_I2C_Mem_Write_IT(&hi2c2, redriver_address, channel_register_address + EQ_CONTROL_REGISTER_OFFSET, I2C_MEMADD_SIZE_8BIT, &eq_index, 1);}static void initialize_channel_rx_detect(uint16_t redriver_address, uint16_t channel_register_address, uint8_t rx_detect) { HAL_I2C_Mem_Write_IT(&hi2c2, redriver_address, channel_register_address + RX_DETECT_CONTROL_REGISTER_OFFSET, I2C_MEMADD_SIZE_8BIT, &rx_detect, 1);}static void initialize_channel_bias(uint16_t redriver_address, uint16_t channel_register_address, uint8_t bias) { HAL_I2C_Mem_Write_IT(&hi2c2, redriver_address, channel_register_address + BIAS_REGISTER_OFFSET, I2C_MEMADD_SIZE_8BIT, &bias, 1);}static void initialize_channel_eq_profile(uint16_t redriver_address, uint16_t channel_register_address, uint8_t eq_profile) { HAL_I2C_Mem_Write_IT(&hi2c2, redriver_address, channel_register_address + EQ_GAIN_FLAT_GAIN_REGISTER_OFFSET, I2C_MEMADD_SIZE_8BIT, &eq_profile, 1);}static void initialize_gpu_cpu_redriver(){ initialize_channel_eq(GPU_CPU_0_3_ADDR_I2C, CHANNEL_0_REGISTER, EQ_CONTROL_EQ_STAGE2_2 | EQ_CONTROL_EQ_STAGE1_2); initialize_channel_eq(GPU_CPU_0_3_ADDR_I2C, CHANNEL_1_REGISTER, EQ_CONTROL_EQ_STAGE2_2 | EQ_CONTROL_EQ_STAGE1_2); initialize_channel_eq(GPU_CPU_0_3_ADDR_I2C, CHANNEL_2_REGISTER, EQ_CONTROL_EQ_STAGE2_2 | EQ_CONTROL_EQ_STAGE1_2); initialize_channel_eq(GPU_CPU_0_3_ADDR_I2C, CHANNEL_3_REGISTER, EQ_CONTROL_EQ_STAGE2_2 | EQ_CONTROL_EQ_STAGE1_2); initialize_channel_eq(GPU_CPU_4_7_ADDR_I2C, CHANNEL_4_REGISTER, EQ_CONTROL_EQ_STAGE2_2 | EQ_CONTROL_EQ_STAGE1_1); initialize_channel_eq(GPU_CPU_4_7_ADDR_I2C, CHANNEL_5_REGISTER, EQ_CONTROL_EQ_STAGE2_2 | EQ_CONTROL_EQ_STAGE1_1); initialize_channel_eq(GPU_CPU_4_7_ADDR_I2C, CHANNEL_6_REGISTER, EQ_CONTROL_EQ_STAGE2_2 | EQ_CONTROL_EQ_STAGE1_1); initialize_channel_eq(GPU_CPU_4_7_ADDR_I2C, CHANNEL_7_REGISTER, EQ_CONTROL_EQ_STAGE2_2 | EQ_CONTROL_EQ_STAGE1_1); initialize_channel_rx_detect(GPU_CPU_0_3_ADDR_I2C, CHANNEL_0_REGISTER, EN_RX_DET_COUNT | SEL_RX_DET_COUNT); initialize_channel_rx_detect(GPU_CPU_0_3_ADDR_I2C, CHANNEL_1_REGISTER, EN_RX_DET_COUNT | SEL_RX_DET_COUNT); initialize_channel_rx_detect(GPU_CPU_0_3_ADDR_I2C, CHANNEL_2_REGISTER, EN_RX_DET_COUNT | SEL_RX_DET_COUNT); initialize_channel_rx_detect(GPU_CPU_0_3_ADDR_I2C, CHANNEL_3_REGISTER, EN_RX_DET_COUNT | SEL_RX_DET_COUNT); initialize_channel_rx_detect(GPU_CPU_4_7_ADDR_I2C, CHANNEL_4_REGISTER, EN_RX_DET_COUNT | SEL_RX_DET_COUNT); initialize_channel_rx_detect(GPU_CPU_4_7_ADDR_I2C, CHANNEL_5_REGISTER, EN_RX_DET_COUNT | SEL_RX_DET_COUNT); initialize_channel_rx_detect(GPU_CPU_4_7_ADDR_I2C, CHANNEL_6_REGISTER, EN_RX_DET_COUNT | SEL_RX_DET_COUNT); initialize_channel_rx_detect(GPU_CPU_4_7_ADDR_I2C, CHANNEL_7_REGISTER, EN_RX_DET_COUNT | SEL_RX_DET_COUNT); initialize_channel_bias(GPU_CPU_0_3_ADDR_I2C, CHANNEL_0_REGISTER, BIAS_CURRENT_0); initialize_channel_bias(GPU_CPU_0_3_ADDR_I2C, CHANNEL_1_REGISTER, BIAS_CURRENT_0); initialize_channel_bias(GPU_CPU_0_3_ADDR_I2C, CHANNEL_2_REGISTER, BIAS_CURRENT_0); initialize_channel_bias(GPU_CPU_0_3_ADDR_I2C, CHANNEL_3_REGISTER, BIAS_CURRENT_0); initialize_channel_bias(GPU_CPU_4_7_ADDR_I2C, CHANNEL_4_REGISTER, BIAS_CURRENT_0); initialize_channel_bias(GPU_CPU_4_7_ADDR_I2C, CHANNEL_5_REGISTER, BIAS_CURRENT_0); initialize_channel_bias(GPU_CPU_4_7_ADDR_I2C, CHANNEL_6_REGISTER, BIAS_CURRENT_0); initialize_channel_bias(GPU_CPU_4_7_ADDR_I2C, CHANNEL_7_REGISTER, BIAS_CURRENT_0); initialize_channel_eq_profile(GPU_CPU_0_3_ADDR_I2C, CHANNEL_0_REGISTER, EQ_PROFILE_3 | FLAT_GAIN_0 | FLAT_GAIN_2); initialize_channel_eq_profile(GPU_CPU_0_3_ADDR_I2C, CHANNEL_1_REGISTER, EQ_PROFILE_3 | FLAT_GAIN_0 | FLAT_GAIN_2); initialize_channel_eq_profile(GPU_CPU_0_3_ADDR_I2C, CHANNEL_2_REGISTER, EQ_PROFILE_3 | FLAT_GAIN_0 | FLAT_GAIN_2); initialize_channel_eq_profile(GPU_CPU_0_3_ADDR_I2C, CHANNEL_3_REGISTER, EQ_PROFILE_3 | FLAT_GAIN_0 | FLAT_GAIN_2); initialize_channel_eq_profile(GPU_CPU_4_7_ADDR_I2C, CHANNEL_4_REGISTER, EQ_PROFILE_3 | FLAT_GAIN_0 | FLAT_GAIN_2); initialize_channel_eq_profile(GPU_CPU_4_7_ADDR_I2C, CHANNEL_5_REGISTER, EQ_PROFILE_3 | FLAT_GAIN_0 | FLAT_GAIN_2); initialize_channel_eq_profile(GPU_CPU_4_7_ADDR_I2C, CHANNEL_6_REGISTER, EQ_PROFILE_3 | FLAT_GAIN_0 | FLAT_GAIN_2); initialize_channel_eq_profile(GPU_CPU_4_7_ADDR_I2C, CHANNEL_7_REGISTER, EQ_PROFILE_3 | FLAT_GAIN_0 | FLAT_GAIN_2);}static void initialize_cpu_gpu_redriver(){ initialize_channel_eq(CPU_GPU_0_3_ADDR_I2C, CHANNEL_0_REGISTER, EQ_CONTROL_EQ_STAGE2_0 | EQ_CONTROL_EQ_STAGE1_BYPASS); initialize_channel_eq(CPU_GPU_0_3_ADDR_I2C, CHANNEL_1_REGISTER, EQ_CONTROL_EQ_STAGE2_0 | EQ_CONTROL_EQ_STAGE1_BYPASS); initialize_channel_eq(CPU_GPU_0_3_ADDR_I2C, CHANNEL_2_REGISTER, EQ_CONTROL_EQ_STAGE2_0 | EQ_CONTROL_EQ_STAGE1_BYPASS); initialize_channel_eq(CPU_GPU_0_3_ADDR_I2C, CHANNEL_3_REGISTER, EQ_CONTROL_EQ_STAGE2_0 | EQ_CONTROL_EQ_STAGE1_BYPASS); initialize_channel_eq(CPU_GPU_4_7_ADDR_I2C, CHANNEL_4_REGISTER, EQ_CONTROL_EQ_STAGE2_0 | EQ_CONTROL_EQ_STAGE1_BYPASS); initialize_channel_eq(CPU_GPU_4_7_ADDR_I2C, CHANNEL_5_REGISTER, EQ_CONTROL_EQ_STAGE2_0 | EQ_CONTROL_EQ_STAGE1_BYPASS); initialize_channel_eq(CPU_GPU_4_7_ADDR_I2C, CHANNEL_6_REGISTER, EQ_CONTROL_EQ_STAGE2_0 | EQ_CONTROL_EQ_STAGE1_BYPASS); initialize_channel_eq(CPU_GPU_4_7_ADDR_I2C, CHANNEL_7_REGISTER, EQ_CONTROL_EQ_STAGE2_0 | EQ_CONTROL_EQ_STAGE1_BYPASS); initialize_channel_rx_detect(CPU_GPU_0_3_ADDR_I2C, CHANNEL_0_REGISTER, MR_RX_DET_MAN); initialize_channel_rx_detect(CPU_GPU_0_3_ADDR_I2C, CHANNEL_1_REGISTER, MR_RX_DET_MAN); initialize_channel_rx_detect(CPU_GPU_0_3_ADDR_I2C, CHANNEL_2_REGISTER, MR_RX_DET_MAN); initialize_channel_rx_detect(CPU_GPU_0_3_ADDR_I2C, CHANNEL_3_REGISTER, MR_RX_DET_MAN); initialize_channel_rx_detect(CPU_GPU_4_7_ADDR_I2C, CHANNEL_4_REGISTER, MR_RX_DET_MAN); initialize_channel_rx_detect(CPU_GPU_4_7_ADDR_I2C, CHANNEL_5_REGISTER, MR_RX_DET_MAN); initialize_channel_rx_detect(CPU_GPU_4_7_ADDR_I2C, CHANNEL_6_REGISTER, MR_RX_DET_MAN); initialize_channel_rx_detect(CPU_GPU_4_7_ADDR_I2C, CHANNEL_7_REGISTER, MR_RX_DET_MAN); initialize_channel_bias(CPU_GPU_0_3_ADDR_I2C, CHANNEL_0_REGISTER, BIAS_CURRENT_1); initialize_channel_bias(CPU_GPU_0_3_ADDR_I2C, CHANNEL_1_REGISTER, BIAS_CURRENT_1); initialize_channel_bias(CPU_GPU_0_3_ADDR_I2C, CHANNEL_2_REGISTER, BIAS_CURRENT_1); initialize_channel_bias(CPU_GPU_0_3_ADDR_I2C, CHANNEL_3_REGISTER, BIAS_CURRENT_1); initialize_channel_bias(CPU_GPU_4_7_ADDR_I2C, CHANNEL_4_REGISTER, BIAS_CURRENT_1); initialize_channel_bias(CPU_GPU_4_7_ADDR_I2C, CHANNEL_5_REGISTER, BIAS_CURRENT_1); initialize_channel_bias(CPU_GPU_4_7_ADDR_I2C, CHANNEL_6_REGISTER, BIAS_CURRENT_1); initialize_channel_bias(CPU_GPU_4_7_ADDR_I2C, CHANNEL_7_REGISTER, BIAS_CURRENT_1); initialize_channel_eq_profile(CPU_GPU_0_3_ADDR_I2C, CHANNEL_0_REGISTER, EQ_PROFILE_0 | FLAT_GAIN_0 | FLAT_GAIN_1); initialize_channel_eq_profile(CPU_GPU_0_3_ADDR_I2C, CHANNEL_1_REGISTER, EQ_PROFILE_0 | FLAT_GAIN_0 | FLAT_GAIN_1); initialize_channel_eq_profile(CPU_GPU_0_3_ADDR_I2C, CHANNEL_2_REGISTER, EQ_PROFILE_0 | FLAT_GAIN_0 | FLAT_GAIN_1); initialize_channel_eq_profile(CPU_GPU_0_3_ADDR_I2C, CHANNEL_3_REGISTER, EQ_PROFILE_0 | FLAT_GAIN_0 | FLAT_GAIN_1); initialize_channel_eq_profile(CPU_GPU_4_7_ADDR_I2C, CHANNEL_4_REGISTER, EQ_PROFILE_0 | FLAT_GAIN_0 | FLAT_GAIN_1); initialize_channel_eq_profile(CPU_GPU_4_7_ADDR_I2C, CHANNEL_5_REGISTER, EQ_PROFILE_0 | FLAT_GAIN_0 | FLAT_GAIN_1); initialize_channel_eq_profile(CPU_GPU_4_7_ADDR_I2C, CHANNEL_6_REGISTER, EQ_PROFILE_0 | FLAT_GAIN_0 | FLAT_GAIN_1); initialize_channel_eq_profile(CPU_GPU_4_7_ADDR_I2C, CHANNEL_7_REGISTER, EQ_PROFILE_0 | FLAT_GAIN_0 | FLAT_GAIN_1);}void initialize_redrivers() { HAL_I2C_IsDeviceReady(&hi2c2, CPU_GPU_0_3_ADDR_I2C, 1024, 1); HAL_I2C_IsDeviceReady(&hi2c2, CPU_GPU_4_7_ADDR_I2C, 1024, 1); HAL_I2C_IsDeviceReady(&hi2c2, GPU_CPU_0_3_ADDR_I2C, 1024, 1); HAL_I2C_IsDeviceReady(&hi2c2, GPU_CPU_0_3_ADDR_I2C, 1024, 1); initialize_gpu_cpu_redriver(); initialize_cpu_gpu_redriver();}