This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS320PR410: Swaping for lane and pin

Part Number: DS320PR410

Tool/software:

Dear Technical Support Team,

I have two questions and confirm the functionality of the Re-driver “DS320PR410RNQR” and “DS320PR810NJXR”.

Q1
Is it acceptable to reverse the P and N connections for each PCIe signal on these Re-drivers?
For example, connecting TXn/RXn signals to TXp/RXp pins, and connecting TXp/RX signals to TXn/RXn pins.

Q2
Is it acceptable to swap the lanes for these Re-drivers?
For example, connecting TX/RX[1], TX/RX[0], TX/RX[3], TX/RX[2] signals to the TX/RX[0], TX/RX[1], TX/RX[2], TX/RX[3] pins

Best Regards,

ttd