Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMUXHS4612: Camera Link Full to MIPI CSI2

Part Number: TMUXHS4612

Tool/software:

Hello E2E Experts,

Good day.

Is there an interface IC that can convert Camera Link Full to MIPI CSI2?

We have a couple cameras feeding an RZ/V2H MPU for a machine vision application where we will do video fusion and object tracking etc..
the main Camera is Camera link 1 FULL which is 3 links 4 channels each 6 bits per channel if memory serves. I think only 64 of the 72 bits are defined. the MPU is MIPI CSI2 4 Lane. and I have 4 of them. MIPI is 8 bits per lane. i haven't done this stuff in a while so I don't recall the data mapping so there may need to be a small amount of buffer to shuffle the bits. 
Was hoping someone may have done a single chip converter able to handle this without having to load an entire frame first. timing is at a premium.
Camera datasheet is shown below.
Regards,
TICSC
  • Hi TICSC,

    You've tagged this to the MUX forum, but I don't see a request for a mux here. Personally, I don't believe we have an IC that convert camera link to MIPI CSI2 though at TI. I'm not sure what team would support such a request so I can't help direct you in the right way either. Sorry.

    Thanks,
    Rami