Part Number: TCAN1051-Q1
Other Parts Discussed in Thread: TCAN1051
Tool/software:
Hi Expert,
My customer is doing communication test as below, but they get error frame sometimes, please help to analyze and give some suggestions.
- There are 9 nodes on the CAN BUS, the length of the BUS is 8m, and the baud rate is 2Mbps.
- When TCAN1051 is in the recessive state we could see that the CANH-CANL is about 2.2V, however, when TCAN1051 is in the dominant state we could see that the CANH-CANL is nearly 1.5V or lower, which we think is the main reason we get such error frames.


- What are the possible reasons for the error frame? How to solve?
- Besides, we notice that this issue is more easily gotten when a large volume of data is transmitting by TCAN1051, what's the source current of TCAN1051 CAN dominant?

Best Regards,
Jack Li