Part Number: TCAL6408
Other Parts Discussed in Thread: TCAL6416, TCAL6416R, TCAL9539, TCAL9539R, TCAL9538, TCAL9539-Q1
Tool/software:
Hi,
Is there an I/O expander IC like the TCAL6408 where the I/O pins are open-drain (the internal MOSFET only pulls low) and the high level is provided by an external pull-up,
so the logic-high voltage can be set to any level rather than being limited to just 1.8 V or 3.3 V?
Thanks!
Jeff