This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSB8020B: Interface forum

Part Number: TUSB8020B

Tool/software:

We built our own PCB with TUSB8020B without EEPROM and without SMBus interface. Unlike the EVAL-Board our solution does not attach the upstream port to the PC until the cfgActive Flag is set via SMB. How is the TUSB8020B in the EVAL-Board configured so that it immediately attach after power on?

  • Hi Hernler:

         Even if  no EERPOM needed, hub should be in I2C mode (SMBUS=H), other wise,  upstream port  will not be connected until the cfgActive Flag is set via SMBUS.

    Best

    Brian

  • Thank you for the answer but I need to know how this is be done in the TUSB8020BEVM. With this eval-board the upstream port is connected as soon as the power supply is switched on. I removed the EEPROM and there is also no SMBUS communication and it still connects. What is the secret behind it? Does it has a programmed OTP? 

  • on EVM, hub is configured  in I2C mode. If there is EEPROM is detected, hub will read EEPROM information, if EEPROM is not detected, hub will load default configuration . Hub can work in default configuration without EEPROM.

    Best

    brian