Other Parts Discussed in Thread: TUSB2036, TUSB8040
Device: TPS2036
Do I have to use a 48-MHz Clock for USB2.0 or does it work also with a 6-MHz Crystal?
I try to built a USB2.0 Hub but it also works with USB1.1
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
the TUSB2036 only supports Full-speed and Low-speed (USB 1.1)
Regards.
Hello Sebastian,
The tUSB2036 can not be modified to support High-Speed.
The HS traffic is controlled by the EHCI architecture and the FS/LS traffic is controlled by the UHCI/OHCI architecture. A USB 2.0 Host/Hub includes both.
You can use the TUSB8040 for SS and HS, below is the link to the device.
Regards.
http://www.ti.com/product/tusb8040