Part Number: TUSB1142
Tool/software:
Hi,
The host unable to recognize USB 3.0 and USB2.0 devices, the SCH as below.

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TUSB1142
Tool/software:
Hi,
The host unable to recognize USB 3.0 and USB2.0 devices, the SCH as below.

Hi,
I have a few comments:
1) What is the CC/ PD controller used in this applications? How is flip handled?
2) Looks like all EQ pins are pulled to ground. Do you have the ability to tune EQ on this board?
3) SSRX1/2 pins have 220nF caps. This value should 330nF.
USB2.0 buses are independent of USB3.x buses. What does the USB2.0 circuitry look like?
Hi,
1. controller is FUSB302B, Flip is up by CPU.
2. Yes, customer can tune EQ and do you have recommendations?
3. will modified.
Hi,
I think we need to address USB 2.0 not functioning before we move forward with looking at the TUSB1142 and USB3.x.
What does the layout look like for USB2.0. Why is this path not working?
Hello,
Closing thread due to inactivity. If you have any follow-up questions or concerns, feel free to reply.