This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ESDS452: ESDS452 8/20µs surge current @ 80°C

Part Number: ESDS452

Tool/software:

Hi again,

The ESDS452 datasheet doesn't specify the temperature derating for the IEEE 61000-4-5 (8/20µs) max surge current.
(It is only given as 18A @ 25°C.)


Is there any data relative to the max 8/20µs surge current at 80°C (or close to 80°C) ?

Thanks in advance!