Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB947-Q1: ds90ub947 pattern using select external clock + internal timing can not work

Other Parts Discussed in Thread: ALP

solved already

  • Hi Jianwei,

    Thanks for sharing this configuration script, I am happy to help review and analyze it.

    Can you please provide the following information to help me understand the system better?

    • Block diagram of the 947-928 devices
    • Display timing specifications

    I will first try to determine if the timing on the display is too strict for the internal clock generation of the 947 PATGEN. I may also be able to provide an example PATGEN script generated from the ALP GUI for the device.

    Best,

    Miguel

  • Hi Jianwei,

    It seems E2E did not attach your latest reply, but I have received the message internally.

    Hi Miguel,
    ok now. update the script
    ub947addr=0x1a
    write_patgen_reg()
    {
    local addr=$1
    local data=$2
    i2ctransfer -f -y 3 w2@${ub947addr} 0x66 $addr
    i2ctransfer -f -y 3 w2@${ub947addr} 0x67 $data
    }
    # static const struct drm_display_mode boe_ae123z7b_l13_wdp2_mode = {
    # .clock = 116985,
    # .hdisplay = 1920, 0x780
    # .hsync_start = 1920 + 70*2, 0x780 + 0x8C
    # .hsync_end = 1920 + 70*2 + 12*2, 0x780 + 0x8C + 0x18
    # .htotal = 1920 + 70*2 + 12*2 + 4*2, 0x780 + 0x8C + 0x18 + 0x08 = 0x82C
    # .vdisplay = 720, 0x2d0
    # .vsync_start = 720 + 207, 0x2d0 + 0xCF
    # .vsync_end = 720 + 207 + 2, 0x2d0 + 0xCF + 0x02
    # .vtotal = 720 + 207 + 2 + 3, 0x2d0 + 0xCF + 0x02 + 0x03 = 0x3A4
    # .vrefresh = 60,
    # };
    #disable pattern
    i2ctransfer -f -y 3 w2@${ub947addr} 0x64 0x10
    # 200Mhz / 2
    write_patgen_reg 0x03 0x03
    #h total[7:0]
    write_patgen_reg 0x04 0x2C
    #v total[3:0]
    #h total[11:8]
    write_patgen_reg 0x05 0x48
    #v total[11:4]
    write_patgen_reg 0x06 0x3A
    #h active width[7:0]
    write_patgen_reg 0x07 0x80
    #v active width[3:0]
    #h active width[11:8]
    write_patgen_reg 0x08 0x07
    #v active width[11:4]
    write_patgen_reg 0x09 0x2d
    #hsw
    write_patgen_reg 0x0a 0x18
    #vsw
    write_patgen_reg 0x0b 0x02
    #hbp
    write_patgen_reg 0x0c 0x08
    #vbp
    write_patgen_reg 0x0d 0x03
    #fps
    write_patgen_reg 0x0f 0x1E
    #select external clock + internal timing
    i2ctransfer -f -y 3 w2@${ub947addr} 0x65 0x0c
    #enable pattern
    i2ctransfer -f -y 3 w2@${ub947addr} 0x64 0x15

    Allow me until EOD / Tomorrow morning to generate a new PATGEN script for you,

    If you have the display timing specifications, would you be able to share them?

    Thanks for your patience

    Best,

    Miguel