Part Number: DS90UB953-Q1
Tool/software:
Dear Team,
if using CLK_OUT when in STP mode and I2C voltage level is 3.3V
IDX 4 -> Vidx target voltage 1.224V -> Rbot= 100k , Rtop = 47k -> I2C 7-bit address is 0x19 , I2C 8-bit address is 0x32
1) Is it ok to use 100k for bottom res and 47k for top res?
2) The top res should be pulled to VDD_1P8_D ( pin25) , 1.8V?
3) When using the CLK_OUT pin with the upper resistors , what is the Vos ( output common-mode voltage) ? is it 1.224V ?
4) When using the CLK_OUT pin with the upper resistors , what is the Vod ( output voltage swing) ?
5) I have to feed this CLK_OUT to a clock input that accepts LVCMOS 3.3V , i assume i will need to do AC coupling and after that bias the signal? What would you propose?
CLK_OUT ( from SER) -> IDX pull-up/down -> AC coupling cap -> resistor bias network with Rt and Rb where Rt pulled to 3.3V -> series resistor -> clk input to the IC
or
CLK_OUT ( from SER) -> IDX pull-up/down -> series resistor -> AC coupling cap -> resistor bias network with Rt and Rb where Rt pulled to 3.3V -> clk input to the IC
Best Regards,
d.