Part Number: TUSB212
Tool/software:
Hi teams,
My customer, LANGO, is using the TUSB212RWBR. They've installed pull-up resistors RU32 = 47K and pull-down resistors RU36 = 47K. I suspect this will cause the chip's DCBOOST/ENA_HS to malfunction. However, several hundred boards have already been shipped to the end customer, and removing components is prohibited, so removing the pull-up resistors is not an option. Is it possible that the redriver won't work with the current configuration? Can adding pull-up resistors (e.g., 1M) resolve this issue? Are there other solutions to resolve this issue without removing components?

Best Regards
Chris