This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TCAN1463-Q1: TCAN1463 vs TCAN1473 behaviour

Part Number: TCAN1463-Q1
Other Parts Discussed in Thread: TCAN1043

Tool/software:

Hello,

I 've analysed TCAN1463 and TCAN1473 datasheets and found no differences in TRCV behavior. Could you clarify the main diff between the devices?

Thank you in advance.

  • Hi Miguel,

    Here is a comparison slide:

    If you are using TCAN1473A, it's basically the same device as TCAN1463, with just a few characteristics updated to meet the CAN SIC specification of ISO11898:2 2024. If you are fine with meeting the CiA 601-4 only (It's also a CAN SIC standard but posted earlier than the ISO11898:2 2024), then TCAN1463 can still be used, there is no functional difference.

    TCAN1473 is like a CAN SIC version of TCAN1043, which has slight difference with TCAN1463/TCAN1473A/TCAN1043A. Thus if you are migrating from TCAN1463/TCAN1043A, TCAN1473A will be the drop in replacement without any software or hardware change.

    Regards,

    Sean

  • Thank you Sean!