This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

THVD4411: THVD4411 for Switch RS232 & RS485

Part Number: THVD4411

Tool/software:

Hi Sir

Did the THVD4411 can achieve it?

Need switch between the RS232 and RS485

  • When RS232 module, Pin define is TX , RX , RTS , CTS
  • When RS485 module, original RS232 TX pin as the RS485的D+,RS232 CTS pin as the RS485 D-
  • Hi Chen,

    Thanks for posting this question.

    THVD4411 can use the same RS-232 pins as the half-duplex RS-485 pins (by connecting R1 and R3). Figure 7-2 and Figure 7-3 in the datasheet show this more clearly. Just note that this will not work for full-duplex RS-485. 

    Best,

    Ethan