Part Number: DS90UB953-Q1
Other Parts Discussed in Thread: DS90UB954-Q1
Tool/software:
Questions:
1. Will this part support 8.3MP camera resolution?
2. Any other part that support voice (I2S) over STP?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DS90UB953-Q1
Other Parts Discussed in Thread: DS90UB954-Q1
Tool/software:
Questions:
1. Will this part support 8.3MP camera resolution?
2. Any other part that support voice (I2S) over STP?
Hello Pichet,
From your question I understood that your interface is MIPI CSI-2, orrect?
What is the data type and frame rate?
What DES are you using?
MIPI CSI-2 interface,
RAW10 or RAW12
3840x2160 @ 30fps, 1920x1080 @ 60fps, 1280x720 @ 120fps
Deserial: DS90UB954-Q1
3840x2160 @ 30fps, RAW10 - Can be supported using the UB953-UB954.
3840x2160 @ 30fps, RAW12 - Can be supported using the UB953-UB954 only if CSI-2 blanking on the Imager is max 10%.
--------
1920x1080 @ 60fps, RAW10/RAW12 - Can be supported using the UB953-UB954.
--------
1280x720 @ 120fps, RAW10/RAW12 - Can be supported using the UB953-UB954.
Is there other part similar to UB953-UB954 with I2S that can deliver RAW12 without blanking?
We do not require or use this blanking. This CSI-2 blanking is generated and used by the image sensor only.
You can use I2S with the UB953-UB954. Refer to this App note: