Tool/software:
How can I estimate the Icc(dynamic) of TRS3122E
when two drivers and receivers are running at 9600bps?
Thanks for your help.
Takashi
Hi Takashi,
This is probably going to depend on the distance of cable you're communicating with. Figure 1 in the datasheet showcases this, at higher datarates you will see a higher current draw. The the X axis, it is your cable distance (longer cable generates a larger capacitive load). An example I like to use is 1m of cat5 cable is about 50pF. So 100m would be around a 5nF load. Using figure 1 at 250kbps you get around a 40mA current draw. You can divide this down by data rate, where 125kbps will get you 20mA and ~60kbps get you 10mA. 30kbps is 5mA. 15kbps is 2.5mA. 7.5kbps is 1.25mA. These all assume your cable is 100m of cat 5 for example....
-Bobby