Part Number: THVD8000
Tool/software:
Hi there
I see in the THVD8000 datasheet there is mention of a bandpass filter on the de-modulator input to the device. I have an application which currently uses two lanes of RS-485 (one for data, the other for a measurement synchronization pulse). I was wondering if it is possible to operate two pairs of THVD8000 on a single twisted pair running at different F_Set values. I assume this would work with a discrete bandpass filter on the input/output but was wondering if the in-built bandpass filter would be sufficient?
Kind regards
Chris