Part Number: MAX3232E
Tool/software:
Hi team,
In the datasheet, Table 9-1 shows the recommended capacitor values versus Vcc. It seems to suggest using different values for Vcc = 5.0 V and Vcc = 3.3 V.
My understanding is that the internal charge pump (doubler) is regulated at ±5.5 V. Therefore, when Vcc = 5 V, the overcharge voltage is higher compared to Vcc = 3.3 V.
This could lead to greater losses than at Vcc = 3.3 V. Is this the reason why a smaller capacitance value is recommended for C1? Is my understanding correct?
I would appreciate your opinion.
Best regards,
teritama