This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PCA9306: Use it like an I2C switch

Part Number: PCA9306
Other Parts Discussed in Thread: TCA9803, LSF0002

Tool/software:

Dear Sirs and Madams,

We would like to use the PCA9306 as an I2C switch.

Therefore, we are considering the following configuration.

Since the I2C bus lines arepulled up to different 3.3V, is it okay to connect VREF1 and VREF2 to 3.3VB?

This is because we want to minimize the number of connection lines between boards.

If the TCA9617 and TCA9803 can be used in a similar way, which device would be best?

Regards,

Masashi