Part Number: TIC12400-Q1
Other Parts Discussed in Thread: TMS570LS0914
Tool/software:
Hello,
I have interfaced this IC with TMS570LS0914 microcontroller. I am checking over voltage condition using this IC.
I am facing below issues :
1. /INT pin does not pull to low on Vs >= 37V.
2. OV flag in INT_STAT register not set to 1 even after OI (other interrupt) condition is triggered.
Below schematic is used. /INT pin is not connected to microcontroller. will that work ?

Configurations and initialization sequence are as below :
1. CONFIG : 0X00
2. IN_EN : 0X00
3. CS_SELECT : 0X3CF
4. WC_CFG0 : 0X249249
5. MODE : 0X00
6. THRES COMP : 0X00
7. CONFIG : 0X800
Reading status at every 100ms interval.
Reading diagnostic at every 100ms interval.
Kindly guide me on this.
Thanks