Part Number: TS3DV642-Q1
Other Parts Discussed in Thread: TS3DV642, , TMUX4827
Tool/software:
Hi,
I have a few questions regarding the TS3DV642 MUX:
From the electrical parameters i deduced that it could also be used for USB2.0 and USB3.0, can TI confirm this?
Also 6 Gbps is it per lane or per total for the entire chip ( aggregate) ? If it is per lane then maybe it can go USB3.1 ?
Since from what i understand it is an analogue MUX can it also be used for analogue audio (single ended and differential ) ? If i have the voltages in the acceptable range. If no what outer type of MUX would you recommend? Low distortion is my requirement insertion loss can be a bit larger if needed.
Also are there any drop in replacements ? pin to pin compatible would be what i need/want. From what i see there are none but i may be mistaken, i need a HDMI 2:1 MUX and i would need at least 2 part numbers for this.
TS3DV642 and TS3DV642-Q1 is not really 2 part numbers in my opinion but it is the best i could find.....
Best regards,
Robert