Part Number: DP83826AE
Tool/software:
My question is not specifically about the DP83826AE (I had to include a P/N to post), but about non-POE Ethernet PHYs in general.
This will seem as an unusual question, but my understanding of Ethernet PHY’s is very limited.
For a non-PoE Ethernet PHY what is the "drive current capability" of most Ethernet PHYs?
My understanding is that for a 10BASE-T the voltage levels are +-2.5V.
The output impedance of Ethernet is 100 ohms, so that gives 25mA = 2.5V/100 ohms
But, 100 meters of CAT5 Ethernet Cable has a resistance of about 10 ohms. So, the Ethernet PHY must be able to supply at least 250mA = 2.5V/10 ohms to support IEEE 802.3 100 meter standards. Is that correct?
What over current protection is built into most non-POE Ethernet PHYs? If you connected all 4 channels to ground would that damage most Ethernet PHYs?
Thanks!