Part Number: AM26C32
Tool/software:
This also applies to other RS485 receiver ICs, 65C1168, for instance.
I note that the output drive on the logic side (not the line driver side) is asymmetric. Datasheets quote Vhi=3.8V, Vlo=0.2V for Vcc=5V. Approximating to a resistor that is 200Ω on the high side and 33Ω on the low side. Is there a reason for this? Are there more symmetric devices?
The reason I ask, is that I am turning a PDM signal back to analogue, and a simple 2-pole filter on the output of the receiver seemed the easiest way, but it needs a symmetric drive.