Other Parts Discussed in Thread: DS90UB954-Q1, DS90UB953-Q1
Tool/software:
I am planning to use the DS90UB953-Q1 Serializer and DS90UB954-Q1 Deserializer along with the AR0341AT camera sensor in my custom board design.
Each camera module consists of an AR0341AT sensor with a 4-lane MIPI CSI interface connected to a DS90UB953-Q1 Serializer. Two such camera modules will interface with the DS90UB954-Q1 Deserializer via the FPD-Link III interface.
The output of the Deserializer will then connect to the i.MX8M Plus processor through the MIPI CSI interface.
I have a clarification — for this setup, should the connection from the processor be configured as a single 4-lane MIPI CSI channel or as dual 2-lane MIPI CSI channels to properly interface with the two camera modules?