Part Number: PCA9306
Other Parts Discussed in Thread: TCA9617B
Tool/software:
Hi Team,
The design has 2 PCA9306 to power 2 devices. They are U102, U108443,
U102 cannot communicate.
Is there a problem with this design?

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Tyler,
Is the connection method shown below feasible?
When using the PCA9306 for level shifting with a 3.3V input signal, does it mean there is no buffer function?
Please recommend an IC that provides both level shifting and buffer functions.



Hi Allen,
PCA9306 is not a true buffer with re-driving circuitry. It is a passive level translator.
A buffer like TCA9617B could work here with VCCA = VCCB = 3.3 V.
However, what is the VIL of the PCIe SW, i2c expander, and BMC?
Can we confirm that BMC VIL = 0.30 x VCC = 0.3 x 3.3 = 0.99 V?
Why do we need level translation if PCA9306 is being used from 3.3V to 3.3V?
Is there a scope capture to capture the fail mode?
Regards,
Tyler