Part Number: DP83867CR
Other Parts Discussed in Thread: DP83867ERGZ-S-EVM, DP83867ERGZ-R-EVM
For the 25MHz external clock inputs, if provided by 3.3V the data sheet (page 116, fig 8.3) recommends a capacitive voltage divider with two 27pF caps. The divider output is straight into the clock input pin XI. This pin has voltage swing requirement of less than 0.45V to over 1.4V. It also has a spec'ed leakage of up to +/-10uA. A possible problem is how this leakage pulls off the DC average of the input so that the swing specs are not met (a simple SPICE sim shows the swing can go out of spec). If there is an internal bias network on the die to prevent this problem, I can find no mention of it in the data sheet. Is there an internal bias network? If not, the possible problem can be headed off with a resistive voltage divider as a mid point bias on the input pin (set to 0.9V at impedance greater than 10k to prevent 10uA from pulling more than 100mV).