Part Number: DS90UB928Q-Q1
Hello team,
Is it okay to input signal to RIN+/RIN- from Ser when Des is power down?
Regards,
Youhei MIYAOKA
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DS90UB928Q-Q1
Hello team,
Is it okay to input signal to RIN+/RIN- from Ser when Des is power down?
Regards,
Youhei MIYAOKA
Hi Youhei,
Yes that is fine.
BR,
Esther
Hello Esther,
Thank you. Is the abs max value related in this topic below highlighted value?

Regards,
Youhei
Hi Youhei,
Yes, please use this to refer to DES input voltages when the DES is powered off. Is there additional DC bias on the FPD-Link?
The SER driving the DOUT voltages should be the recommended operating conditions for DES RX, and it is fine to apply this before DES powers up to fulfill power sequencing. Please note these are absolute maximum ratings, which are fine as long as the DES is not powered on (during function).
Best,
Miguel