This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TCAN1462-Q1: Requirement

Part Number: TCAN1462-Q1

Hi team,

TCAN1462 can follow the 4 requirements?

Transmission rates and .
 Frame format
1) the communication speed in the arbitration area should be 500 kbps +/- 0.3%.
  2) the communication speed of the data area must be 2 Mbps +/-0.3%.
  3) Hardware that can change the transmission speed of the data area to 500 kbps and 1 Mbps.
  4) All messages that can be sent by DUT must be hardware that can be configured as 11-bit standard format specified in the bit assignment table or as an extended format for 29-bit ID.
Synchronization settings Can clock frequency 40MHz
Settings area Arbitration area Data area
Transmission rate 500 Kbps 2 Mbps
Bit Time (NBT) 80 TQ 20 TQ
Sample point 80% 70%
Sync_Seg 1 TQ 1 TQ
Prop_Seg 47 TQ 7 TQ
Phase_Seg1 16 TQ 6 TQ
Phase_Seg2 16 TQ 6 TQ
Sync Jump Width (SJW) 16 TQ 6 TQ
Sample Count (SAM) Once Once
Bit synchronization method Recessive to dominant Edge only
Secondary sampling point - 70%

Best,

Shoo