Part Number: SN74AXC8T245
Other Parts Discussed in Thread: TXV0108
Hi,
For our next gen SoC product (in the market in 1+years), I am looking for a component which can help do a board level voltage level conversion between 1.2V <-> 1.8V for interfaces like RGMII at 125Mhz or OSPI DDR at 200Mhz. The high level issue is that in advanced technologies, it is easier to support 1.2V IO than 1.8V IO.
- I was looking at SN74AXC8T245 from TI: the data sheet says “Up to 380Mbps support when translating from 1.8V to 3.3V”. What is the data speed from 1.2V to 1.8V and 1.8V to 1.2V? Does 380mbps for 8 bits means that a single bit can only be translated at a max of 47.5mhz?
- Do you see any speed impact (or any impact for that matter) for a protocol with bi-direction signals (going from master -> slave and slave -> master in a single clock) translating between 1.2V & 1.8V or is the max speed only able to hit for a protocol in which all the signals go in a single direction (master -> slave or slave -> master) on one clock?
- Can you suggest if TI may have some other part which is more suited to my needs and the rough retail cost for that part?
Thanks for your inputs!