Part Number: CD74HC4067-Q1
Hello team,
We have some questions when use the part in ZCU, kindly ask your insights.
1. The chip is powered by 5V, and the input pin receives 3.3V. After the channel is enabled, a 5.3V level appears at the COMMON port. What could be the reason?
2. Is there any problem if analog and digital signals are mixed on adjacent input ports? The isolation between adjacent channels should be fine, right?
3. For unused input pins, should they be left floating or connected to ground?
BR,
Daniel