This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TXG4041-Q1: Max Leakage Current

Part Number: TXG4041-Q1

All, 

My customer has the following question: 

We are looking at your ground-level translator product line.  It looks like they can support +/- 10V, +/- 40V or +/- 80V of ground isolation and have multiple amounts of digital IO.

 

I have attached the datasheet for your 4 bit +/- 40V part that can support +/- 40V of DC ground shifts.

 

My question is regarding your specification for leakage between the two grounds internal to this part.

 

 

These currents are specified with VCCA and VCCB from 1.71 to 5.5V.

 

I would like to know what the max leakage current is between the grounds when there is +40 and -40V between them?

 

Our application needs a certain amount of isolation between these grounds so this current is important to us.

 

Regards,

Aaron