Part Number: TCA9801
Other Parts Discussed in Thread: ISO1540,
Hello,
I have an I2C circuit with a TCA9801 buffer and an ISO1540 buffer connected to each other. During a high-to-low transition, from the ISO1540 buffer, to the TCA9801, I'm seeing an unexpected low pulse on the SDA line. The ISO1540 is specifically designed to produce an output low level of about 570mV, in order to avoid triggering its own input circuitry. So, I'm wondering if this unexpected low pulse, which drives the SDA line down near zero volts, could cause the I2C bus to lock up. See attached pdf for more detailed information.I2C_buffer_ISO1540_to_TCA9801_issue.pdf