This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TCA9511A: Rise-Time Accelerator Hysteresis

Part Number: TCA9511A

For the TCA9511A, the rise time accelerators specify a 0.6 V threshhold and a slew-rate requirement to trigger. I am curious how sensitive the accelerators are to non-monotonic edges around this threshhold voltage and assuming the slew rate requirement is met. 

Is there anything else in the RTA circuit such as hysteresis that would reduce the possibility of these firing off on a falling edge that is non-monotonic around this 0.6 V threshhold?

Thanks.

  • Hello Ryan,

    We are looking into your question and will respond soon. Thanks!

    Regards,

    Josh

  • Hi Ryan,

    Are you seeing non-montonic edges when using the TCA9511A? 

    My theory is that you wouldn't see non-monotonic edges in the first place since if you do trigger the RTA (with 0.6V threshold and slew rate) then you will see an immediate pull-up current assistance of typically 5 mA towards the supply. The rising edge doesn't seem to have a chance to rise-fall-rise due to the RTA's in the device. 

    Regards,

    Tyler

  • The TCA9511A hasn't been implemented yet, but the product is very risk adverse, so I am trying to verify its operation prior to committing to a design.

    The rising edge does not concern me, it's the falling edge that raises concern. Due to the open-drain configuration, these edges tend to be fast. The RTA also provides good immunity against EMI on the rise, but the RTA doesn't help the fall.

    It is unclear to me if the RTA could fire off if it bounced say from 0.55 V to 0.65 V during a falling transition.  

  • Hi Ryan,

    From an internal spec point of view, I was not able to find a set hysteresis around the RTA trigger threshold of 0.6 V. 

    I would need to confirm with our design team to understand this further. Is this information needed to design in the device and if so how fast do you need the info? 

    Regards,

    Tyler

  • Hi Tyler, 

    This is something that I have to thoroughly investigate to meet customer requirements. If you can reach out to the design team and have an answer by the end of the week, that would be very helpful. If it will take longer, please let me know, but I understand everyone is busy in the world.

    I also started this thread in case anybody had this question in the future.

    Thanks for your help.

  • Hi Ryan,

    I pinged our design team to double check. It might take till beginning of next week to get a complete answer. 

    Regards,

    Tyler

  • Great. Thanks for letting me know.

  • Hi Ryan,

    You're welcome. I'll respond back asap. 

    Regards,

    Tyler

  • Hi Ryan,

    I checked with our design team and got some results. 

    THe TCA9511A one-shot behavior does not have hysteresis at the comparator input. There is a 15ns glitch filter at the output however. This should handle small glitches and small non-monotonic behavior. 

    If you have more details on the glitch height and width of the non-monotonic behavior you expect, design is willing to help simulate specific use cases. 

    Regards,

    Tyler

  • Hi Tyler,

    Thank you for the response - it is helpful to know there is a glitch filter.

    In other product tests, we have seen short ~1ns glitches up to 100mv, but we were able fix those through design changes. Unless we see concerning behavior during our test procedures (which will be several weeks from now), I am going to consider this question answered. I believe that from a probabilistic perspective, the concern for a false trigger is very low anyway, but we want to address any concerns our customers raise. 

    Let the design team know I appreciate their willingness to simulate.

    Thank you for all your help,

    Ryan