Part Number: TUSB4041I
Hi Team,
Can you please provide a Certificate of Volatility for TUSB4041I?
Thanks,
Marvin
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TUSB4041I
Hi Team,
Can you please provide a Certificate of Volatility for TUSB4041I?
Thanks,
Marvin
Hi Ryan,
I was looking at the datasheet and noticed the part had some OTP ROM as well as configuration registers and endpoint buffers. I have a few questions regarding those sections. What size is the OTP ROM? For the registers, can defaults be programmed on the chip without having an external EEPROM? If so, how many bytes can be written to internal EEPROM for that config? The are the endpoint buffers on the chip? If so, what size are they and do they clear all data when the chip powered down?
Thanks,
Jason
Hi Jason,
The OTP ROM for this device is 8 bytes, and typically cannot be programmed directly.
There is no internal EEPROM for this device, an external EEPROM would need to be used for any register configuration on start-up.
Any information written to the TUSB4041I will be cleared on reset, and then read from the external EEPROM on start-up.
Thanks,
Ryan
Hi Ryan,
Thanks for the additional information. Ok so to be clear, is the 8 byte OTP user programmable at all? Can you also speak to the endpoint buffers as to size and volatility? Do these buffers clear on power down?
Thanks,
Jason
Hi Jason,
I am checking internally on the endpoint buffers, I am not totally familiar with these. As for the 8 Byte OTP, these are programmed at the factory and cannot be programmed by the user.
Thanks,
Ryan
Hi Jason,
There are endpoint buffers on the TUSB4041I, these are non-voltatile and 64 bytes. On power down, these buffers clear, yes.
Thanks,
Ryan
Hello,
Closing thread due to inactivity. If you have any follow-up questions or concerns, feel free to reply.
Thanks,
Ryan