Part Number: SN65LV1023A
Other Parts Discussed in Thread: SN65LV1224B,
Does anyone have any experience using SN65LV1023A and SN65LV1224B serializer/deserializer devices as replacements for MAX9205 and MAX9206 devices, which are now obsolete?
We currently use the Maxim parts in a short serial data link systems using a TCLK/REFCLK frequency of approximately 19.6MHz, so well within the frequency range of the TI parts..
Comparing the specifications, they look very close. We're aware of the difference in REFCLK tolerance (100ppm for the SN65LV1224B compared to 200ppm for the MAX9206) and there's also a small difference in threshold on the LVDS input, but we're wondering if anybody knows of any other differences in operation that might cause difficulty.
This is a relatively old product, so ideally we don't want to make major changes, but small hardware modifications if required to accommodate the SN65LV1023A and SN65LV1224B would be OK.
Best regards
Simon