Part Number: DP83867ERGZ-S-EVM
Other Parts Discussed in Thread: DP83869, DP83867CS
Hello TI Support Team,I’m working with the DP83867ERGZ PHY connected to an NXP SJA1110 Ethernet switch through an SGMII (4-wire) interface. The MDIO of the PHY is also controlled by the SJA1110.I’d like to confirm the correct configuration and driver setup for operating the PHY in this mode. Specifically, I’m looking for:A reference driver or initialization example for the DP83867 operating in SGMII-to-100BASE-TX mode.A version that is standalone (non-Linux / non-RTOS / non-AUTOSAR).Details on any special register settings or sequences needed to ensure successful SGMII auto-negotiation and link-up with the SJA1110.Any available documentation or example code for this configuration would be very helpful.Thank you,
Abdullah Eid