Part Number: SN65DP141
The datasheet for the SN65DP141 has the typical and max power dissipation for 4 channel active. Do you have typical/max power dissipations for 3.3VDC VCC with 1 or 2 channel active?
Thank you.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: SN65DP141
The datasheet for the SN65DP141 has the typical and max power dissipation for 4 channel active. Do you have typical/max power dissipations for 3.3VDC VCC with 1 or 2 channel active?
Thank you.
Hi Zach,
We have collected this data for typical some time ago:
@3.3V + VOD=LOW:
0 channel on: 0.006108 A => 20mW
1 channel on: 0.036180 A => 119mW
2 channel on: 0.066200 A => 218mW
3 channel on: 0.096480 A => 318mW
4 channel on: 0.127050 A => 419mW
Please note that changing EQ setting does not change the power consumption much (~3mW).
Please let me know if you have any questions.
Best,
J