Other Parts Discussed in Thread: DS22EV5110, DS34RT5110
Hello,
I need to use DS634RT5110 or DS22EV5110 component. I would like to know if it exists an extended operating temperature range for these components (on -40°C to 85°C; they are specified for 0°C to +70°C). Else, does it exist an "equivalent" component specified for this temperature range [-40°C ; +85°C] ?
Thanks.
Mathieu